Drive_Homing_Inputs_Setting
Index.Sub | 2081.0H | ||||||||||||||||||||||||||||||||||||
Data Type | Unsigned32 | ||||||||||||||||||||||||||||||||||||
Access | Read/Write | ||||||||||||||||||||||||||||||||||||
PDO Mappable |
RX_PDO (1) |
||||||||||||||||||||||||||||||||||||
Unit | -- | ||||||||||||||||||||||||||||||||||||
Range |
0 ÷ FFFFFFFFH | ||||||||||||||||||||||||||||||||||||
Default Value | 00000000H | ||||||||||||||||||||||||||||||||||||
Store Supported | Yes (2) | ||||||||||||||||||||||||||||||||||||
Description |
This object is used to define drive digital inputs Bank #0 allocation forHoming mode (hm). For any function can be assigned one digital input that have to be specified in the four bits of the object concerning that function.
0 = B0_IN0 digital input 4 = B0_IN4 digital input 1 = B0_IN1 digital input 5 = B0_IN5 digital input 2 = B0_IN2 digital input 6 = B0_IN6 digital input 3 = B0_IN3 digital input 7 = B0_IN7 digital input |
||||||||||||||||||||||||||||||||||||
Notes |
(1) available with firmware V03r05 or superior. (2) ‘Store supported’ is available with firmware V01r36 or superior. |